Technical FAQs

Ask a Question

Osisense XC_IP protection degree of ZCKE62 and ZCKE67 heads?

Please note that a head sold separately cannot have a IP level because the IP test concerns a complete switch body + head assembled. The IP degree of protection concerns only sub-assemblies with electrical parts.
Attached the datasheet of the ZCKE62 head which does not give any IP value, confirming this point.
So the answer is : please refer to the IP degree of the complete limit switch series = XCKJ which is IP66 rated.
 
Was this helpful?
What can we do to improve the information ?