Technical FAQs

Ask a Question

What is the purpose of the unlock option in the Data Editor

Goals and Symptoms
What is the purpose of the unlock option in the Data Editor

Facts and Change
Unity version 8 and above..

Causes and Fixes
In Unity Pro V8.0 and V8.1, if you right-click in the body of the Data Editor (variables), the last item in the menu drop
down list is 'Unlock'.  The selection is greyed out.  Information on it's purpose cannot be found inthe help.

The unlock option in the Data Editor is only applies a Unity application that is created by the PES software.
It is used to unlock the GenLock placed on the application by PES.

 
Was this helpful?
What can we do to improve the information ?