Technical FAQs

Ask a Question

Power Monitoring Expert 7.2.2 Web Application small report library window

The report library window within the Reports tab in Web Applications is observed to be small as seen in the image below.

Product Line
Power Monitoring Expert 7.2.x
Web Application, Reports, Internet Explorer 11
This is caused by an incompatibility of Microsoft’s Internet Explorer 11 browser with StruxureWare Power Monitoring Expert 7.2.2.

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

  1. Navigate to the ‘Default.aspx’ file located in  “....\Power Monitoring Expert\Web” directory and open it with notepad. (Create a backup of 'Default.aspx' file to be safe)
    By default, the directory is located in “C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Web” 
  2. Change the following line from:
      "<meta http-equiv="X-UA-Compatible" content="IE=edge" />"
    "<meta http-equiv="X-UA-Compatible" content="IE=9" />" 

    (Essentially the word "edge" is replaced with the number "9" )      
  3. Save the file and re-launch Web Application. 
The report library window should appear as in the screenshot below:
Was this helpful?
What can we do to improve the information ?