Technical FAQs

Ask a Question

Preventa XCS_Which XPS safety unit it is that I can associate with the XCSDMP or XCSDMC or XCSDMR magnetic switches

Please find attached a synthesis document showing all the possible XPS association with the XCSDMP or XCSDMC or XCSDMR magnetic switches, depending on the stop category 0 (immediate switching off) or category 1 (time delayed switching off) and on the switch model. Possible selection of XPS units in this document : safety relays, safety controllers.
Was this helpful?
What can we do to improve the information ?