Technical FAQs

Ask a Question

Do we offer an M221 controller with 120 VAC to the discrete input logic?

No, all of our M221 controllers discrete input logic voltages are 24VDC. However, the controllers can have a digital input expansion module with AC input (120 VAC) such as the TM3DI8A.
Was this helpful?
What can we do to improve the information ?