Technical FAQs

Ask a Question

Why can't I connect to my Quantum processor over Modbus serial?

If the Quantum processor has a running program there maybe an XMIT block be executed. If there is an XMIT in the project it takes control of the Modbus port and you will not be able to connect. If you want to connect over modbus the XMIT block must be disabled by connecting with another protocol first.
Was this helpful?
What can we do to improve the information ?