Technical FAQs

Ask a Question

Osisense XC_Can you supply the complete XCKJ20511 limit switch?

Please note that the complete XCKJ20511 limit switch can be ordered in complete switch since some years. XCKJ20511H7 version is available too. Both references are not in stock, they are produced at order reception by the assembling plant in France. If you need it urgently, you can order the corresponding sub-assemblies ZCKJ2 contact body + ZCKE05 rotary head + ZCKJ11 plastic roller lever, available in stock, and assemble them to get the complete reference.
Was this helpful?
What can we do to improve the information ?