Technical FAQs

Ask a Question

140DRA84000 with CableFast

Issue:
Can I use the 140DRA84000 with CableFast?

Product Line:
Quantum

Resolution:
Yes. The 140DRA84000 is compatible with CableFast part number 140CFA04000.
When using this CableFast block you are limited to 0.5A per point. 150VAC/150VDC max.
Was this helpful?
What can we do to improve the information ?