Technical FAQs

Ask a Question

How to do silent installation of Unity Pro Hotfixes?

It is possible to launch installation of several HotFixes automatically (in a silent way).
For that:

Edit the registery and add following key:
- For a 32-bit OS, XP, W7 or W8.x, type:
if it does not exist, add thekey HKEY_LOCAL_MACHINE, "SOFTWARE\Schneider Electric\Common\UnityProHotfix\,
in this key, add value "SilentMode" with data set to "ON"
- For a 64-bit OS W7 or W8.x, type:
if it does not exist, add the key HKEY_LOCAL_MACHINE, "SOFTWARE\Wow6432Node\Schneider Electric\Common\UnityProHotfix\,
in this key, add value "SilentMode" with data set to "ON"
 
Copy the Hotfix .exe on a Server reachable by the PC or in a directory of the PC.
 
Create a .bat file launching the .exe files running the hotfixes with “/auto” parameter:
            For example if the HotFixes are stored on the PC in the directory c:\Temp        
c:\Temp\UnityPro_V81_HF0273298R.exe /auto
c:\Temp\UnityPro_V81_HF0276305R.exe /auto
c:\Temp\UnityPro_V81_HF0287960R.exe /auto
 
For example if the HotFixes are stored on server:
In this case copy of the HF on the local PC has to be done. 
Copy S:\Technical_Support\Temp1\*.* c:\Temp2
c:\Temp2\UnityPro_V81_HF0273298R.exe /auto
c:\Temp2\UnityPro_V81_HF0276305R.exe /auto
c:\Temp2\UnityPro_V81_HF0287960R.exe /auto
 
Note :  A log file for each HotFixe installed is created in  %TEMP%  directory   in order to be able to verify
           that installation has been done correctly.
 
Was this helpful?
What can we do to improve the information ?