Technical FAQs

Ask a Question

Osisense XC_Datasheet of the XCPR2939P20 limit switch with reset function

Please find attached the datasheet of the XCPR2939P20 limit switch with reset function, not shown into the catalogue. It is a special one designed on request.
Was this helpful?
What can we do to improve the information ?