Technical FAQs

Ask a Question

How do you set the IP Address of a M340 BMXNOE?

To set the IP Address to a M340 BMXNOE01x0 module, a new network needs to be setup. In the Unity project browser, expand the Communication folder then right click on Networks and select New Network…

 
Set up an Ethernet network and name it. The default name is Ethernet_1. Click OK. You will see Ethernet_1 under your Networks folder. Double-click the Ethernet_1 network and the configuration screen will appear.
Within the Ethernet network configuration the appropriate Model Family needs to be selected. The default Ethernet model family is set to a NOE. Leave the default selection. If you hover over the different model family options with your mouse you will see what each option covers as far as CPU's and NOE's.


Once the correct model family has been selected, the new network has to be linked to the BMXNOE. To link the network, select the BMXNOE Ethernet port from the Project Browser. The BMXNOE Ethernet Configuration screen will come up. On that screen you will link the network previously setup, as seen below.


Rev Date 7/18/2017
 
Was this helpful?
What can we do to improve the information ?