Technical FAQs

Ask a Question

Who Supports the Anybus X Gateways ?

Anybus X gateways are made by HMS Industrial Networks a CAPP partner of Schneider Electric.

Many part numbers exist, depending the two fieldbus types a customer wishes to connect.  HMS needs to be consulted for the right one.

Our website shows the following European contact person:

HMS Industrial Networks Partner profile Products  
    Mr Axel Kaiser       
    Emmy-Noether-Str. 17       
    Karlsruhe     76131 Germany     
    Tel.  +49 721 989 777 213            Fax  +49 721 989 777 010     
    axk@hms-networks.de      

In USA, the HMS person, based in Raleigh, is:

Steve Ewankowich        
steve.ewankowich@hms-networks.com    
Business Development, Americas
Office:  312-829-0601

Depending on the customer's location, one of the contacts listed above may be referred to.

These products are offered directly from the partner, not resold by SE at this time.
 
Was this helpful?
What can we do to improve the information ?