Technical FAQs

Ask a Question

Can BPH motors be used with the Lexiium 32 Servo drives?

Yes, the BPH motors are compatible with Lexium 32 servo drives. They are to be characterized as third party motors.  If using a BPH motor with resolver, you will need to use a resolver option card P/N : VW3 M3 401. If using a BPH motor with encoder feedback, you will need to use an encoder option card.VW3 M3 403 (for hiperface encoder) along with a Lexum 32 modular drive (32M). The third party motor commissioning tool within SoMove helps calculate the offset to commutate the motor.
Was this helpful?
What can we do to improve the information ?