Technical FAQs

Ask a Question

PSE 7.4 Event will not Trigger and Cannot be Added to the Computer Setup Wizard

Events added to the Computer Setup Wizard do not save and are not executed during runtime. The name of the event was copied from Excel and pasted in the Project Editor Events Window.

StruxureWare SCADA Expert


When copying from excel there are at least two was to copy the information:
1) Highlight the cell with the desired name and copy the cell
2) Highlight just the text in the cell.
Method 1 will include hidden characters that are added to the name filed. These additional characters will cause the event to not trigger nor be added to the Computer Setup Wizard.

Rename the event in the Project editor to remove the hidden characters.
Was this helpful?
What can we do to improve the information ?