Technical FAQs

Ask a Question

What is the default IP address for the Advantys ETB modules?

The default IP address for the ETB's are 192.168.1.1
Was this helpful?
What can we do to improve the information ?