Technical FAQs

Ask a Question

What is the pin assignment of the RS485 modbus connection on the Schneider Electric adapter TCSMCNAM3M002P ?

Pin 4 of the RJ45 connector is MOD_D1
Pin 5 of the RJ45 connector is MOD_D0

Attached you will also find the pin assignment of the RJ45 ModBus connection of the TCSMCNAM3M002P



 
Was this helpful?
What can we do to improve the information ?