Technical FAQs

Ask a Question

When using the BMXAMI0410 as a 4-20mA input in default mode, what will the module report when operating in an under range condition?

  Here are the values shown in the %IW between 0-4 mA.

  3.99 mA..................-5
  3.50 mA................. -313
  3.00 mA ................ -625
  2.50 mA ................ -800
  2.00 mA................. -800
  1.50 mA ................ -800
  1.00 mA................. -800
  0.50 mA.................- 800
  0.00 mA.................- 800
Was this helpful?
What can we do to improve the information ?