Technical FAQs

Ask a Question

Does the HMIG3U support an ethernet ring topology?

Issue:
Does the HMIG3U support an ethernet ring topology?

Product Line:
HMIG3U

Environment:


Cause:


Resolution:
HMIG3U does not support an ethernet ring topology.  The purpose of the dual ethernet on the HMIG3U is to put the target on two separate networks.
Was this helpful?
What can we do to improve the information ?