Technical FAQs

Ask a Question

How do you set up filtering on an Advantys STBACI1230 module

To filter the STBACI1230 the filtering is performed through the avereging you can average 1 to 8 counts that is selectable. If you double click on the module under parameters you will see averaging and it will average between 1 and 8 samples.
Was this helpful?
What can we do to improve the information ?