Technical FAQs

Ask a Question

Video: How do I print my ladder logic networks in ProWORX 32?

In order to print your ladder logic networks from within ProWORX 32, you must first set the report parameters.

1 - From the main toolbar, go to FILE then REPORT SETUP.
2 - Under the Report Options select Networks.
3 - To print all the networks in the program, click the TOGGLE ALL button.
4 - Click the Save Settings button to save the Report Setup options. Then click the CLOSE button.
5 - From the main toolbar, go to FILE then PRINT.
6 - The Print Setup window will open. Select the printer location and then click the OK button.

Was this helpful?
What can we do to improve the information ?