Technical FAQs

Ask a Question

What is the replacement part number for a Gear box bearing part number GBX0600120701?

Title: What is the replacement part number for a Gearbox bearing part number GBX0600120701?

Issue: Replacement

Product Line: Lexium 32, BMH/BSH motors

Environment: Not applicable

Cause: Obsolescence or change in part numbering scheme

Resolution:  GBX0600120701 can be longer be ordered as a single unit. This is planetary style gear box with a reduction ratio of 12:1. The gear box  with GBX060 012K needs to be ordered for the required reduction ratio. Depending on the associated servo motor that it is to be used with, the corresponding adapter kit needs to be ordered separately.
The chart below shows the ordering scheme for the adapter kit.
Was this helpful?
What can we do to improve the information ?