Technical FAQs

Ask a Question

What is the replacement part number for a Stepper Motor with type code VRDM3913/50LWCEO and part number 52527035600?

Title: What is the replacement part number for a Stepper Motor with type code VRDM3913/50LWCEO and part number 52527035600?

Issue: Replacement

Product Line: VRDM Stepper Motors

Environment: Not applicable


Cause: Obsolescence or change in part numbering scheme


Resolution: The replacement part number for a VRDM 3910 motor with part number V
VRDM3913/50LWCEO bearing part number 52527035600 is  
BRS39BW461ACA. This is an exact replacement motor.
 
Was this helpful?
What can we do to improve the information ?