Technical FAQs

Ask a Question

Osisense XU - Ecolab certificate of compatibility between Ecolab hygiene products and Telemecanique Food and Beverage processing series photo-electric sensors XUK*S rated IP69K

Please find attached our Ecolab certificate of compatibility between the Ecolab hygiene products (P3-topax for example) and Telemecanique Food and Beverage processing series photo-electric sensors XUK*S rated IP69K, and using stainless steel AISI 316L. Such sensors are sold under the references summarized into the following application leaflet Osisense XUKS.
http://download.schneider-electric.com/files?p_File_Id=682842640
Was this helpful?
What can we do to improve the information ?