Technical FAQs

Ask a Question

Is the new Unity Momentum Ethernet port Half or Full duplex?

The new Unity Momentum RJ45 Ethernet 10/100 Mb/s port is Auto duplex (Half or Full)..
Was this helpful?
What can we do to improve the information ?