Technical FAQs

Ask a Question

Can you modify the transmit wait time on Modbus/RTU driver of Vijeo Designer?

Issue:
Can you modify the transmit wait time on Modbus/RTU driver of Vijeo Designer?

Product Line:
Vijeo Designer

Environment:


Cause:


Resolution:
Yes, in Vijeo Designer programming software, there is a field called "TX Wait Time" for the Modbus RTU driver.  This will allow you to change the transmit wait time before sending another request to the device.  Below is a screenshot of that setting in Vijeo Designer.

Was this helpful?
What can we do to improve the information ?