Technical FAQs

Ask a Question

How many panel pages a Magelis screen could have?

Issue:
How many panel pages a Magelis screen could have?

Product Line:
Vijeo Designer, Magelis

Environment:


Cause:


Resolution:
The number of panels that can be created in a project depends on the amount of flash memory available on your target machine and on the size of  each panel. For example, you can have a project on an XBTGT6330 target that contains 100 panels.

As the number of panels for your project increases, memory consumption also increases.
Was this helpful?
What can we do to improve the information ?