Technical FAQs

Ask a Question

Is there a formula for calculating how much data storage will be consumed based on Vijeo Designer data log settings?

Issue:
Is there a formula for calculating how much data storage will be consumed based on Vijeo Designer data log settings?

Product Line:
Vijeo Designer

Environment:


Cause:


Resolution:
There is no simple formula for the calculation of the dataloggging feature in Vijeo Designer. The datalogging are not only accumulate the ASCII characters, but is also use a database with strict structure to store and maintain the datalogging base on the OS. For instance, datalogging also record timestamp and data quality label, as well as any other necessary data involved in the DAT file and other system files.

So it's not easily calculate this by multiply seconds, minutes, etc. The best way to control this is to read from the Vijeo Designer software estimation, and it is the only benchmark you can go by at this time. 
Was this helpful?
What can we do to improve the information ?