Technical FAQs

Ask a Question

What is the difference between Windows Server 2008 R2 and Windows Server 2012?

A lot of functions were added in the newer Win Server OS, some examples below:
· No more Std and Ent SKU, all Win Server 2012 SKUs are with functions like Ent SKU, and Win Server 2008 R2 only supports Std functions.
· Win Server 2008 R2 is without Hyper V, Win Server 2012 default supports Hyper V.
· …

You may check attached file for further details comparison between Win Server 2008 R2 and Win Server 2012.

Was this helpful?
What can we do to improve the information ?