Technical FAQs

Ask a Question

Can a M580 PLC be setup as a NTP server?

Title
M580 NTP Service
 
Issue
Explain M580 NTP Server capability
 
Product Line
M580
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Yes, When the M580 is configured as an NTP server, it can synchronize client NTP clocks (such as a BM• CRA 312 00 adapter). The CPU's internal clock is then used as reference clock for NTP services.

 
Was this helpful?
What can we do to improve the information ?