Technical FAQs

Ask a Question

Will any of the Magelis HMI screens support Dynamic DNS services?

Title
Magelis HMI support for Dynamic DNS services
 
Issue
Identify which Magelis HMI screens support Dynamic DNS services
 
Product Line
Magelis iPC (Panel PC and Box PC)
 
Environment
Vijeo Designer
 
Cause
N/A
 
Resolution
 The Dynamic DNS service should work on our Magelis iPC (Panel PC and Box PC) that running with Windows Full because it is managed by Windows services.
Was this helpful?
What can we do to improve the information ?