Technical FAQs

Ask a Question

When new profile is created in Unity pro Security Editor (example : MySuperProfile), the users associated to this new profile does not have right to add or update DTM in configuration.

To enable right to add or update DTMs in configuration :

Find on computer the file ..\ProgramData\Schneider Electric\Unity Pro\Private\FDTDTMMgr.dll.config

Edit the file with Notepad

After the line

<DtmUserRole unityProfileValue="DefaultValueForCustom" unityProfileName="Custom profile" dtmUserRoleValue="4" dtmUserRoleName="SystemOperator"/>

Add a new line :

<DtmUserRole unityProfileValue="MySuperProfile" unityProfileName="MySuperProfile" dtmUserRoleValue="1" dtmUserRoleName="Administrator"/>

Save the file.

Now the new user with the new profile can add or update the DTM in Unity Pro.

Was this helpful?
What can we do to improve the information ?