Technical FAQs

Ask a Question

QEIO Ethernet Interlink cables

QEIO Ethernet Interlink cables:
Required for an architecture with combined Ethernet RIO and Ethernet DIO devices.
To be connected between the Ethernet 140NOE771xx communication module and the 140CRP31200 head adaptor.
Cable Length 1 m

Standard version TCSECN3M3M1S4
UL version TCSECN3M3M1S4U

Was this helpful?
What can we do to improve the information ?