Technical FAQs

Ask a Question

ION 86XX series power meters socket sealing ring dimensions

User has installed a 3rd party switchboard and requires ION 8600 series sealing rings that are deeper than the 5/8” standard size.

Product Line
ION86xx series power meters

Utility metering offer

A customer may require ION8600 sealing rings that are deeper in size for installation with other 3rd party devices

The standard size of the ION 86xx series meters sealing rings is 5/8" wide in the interior. The socket sealing rings are not manufactured in any other dimensions according to the manufacturer.

Was this helpful?
What can we do to improve the information ?