Technical FAQs

Ask a Question

ION 8650 switchboard meter input current burden at 5A

Issue
User is looking for the input current burden rating at 5A per phase for the PowerLogic ION 8650 switchboard meter. This data is not found in the meter’s datasheet.

Product Line
ION8650 switchboard series power meter

Environment
Utility metering offer

Cause
A customer may require the input current burden rating of the ION8650 switchboard meter to be incorporated in technical design data.

Resolution
The ION 8650 switchboard meter input current burden rating is 1.25VA per phase at 5A.
Was this helpful?
What can we do to improve the information ?