Technical FAQs

Ask a Question

ISO 17025 certification for calibration equipment used for PowerLogic ION meters

Issue
Customer would like to know whether the PowerLogic ION meters’ calibration equipment is ISO 17025 certified

Product Line
PowerLogic ION Meters

Environment
Basic, Intermediate and Advanced metering offers

Cause
Customer is unable to find certification for Schneider Electric’s calibration equipment used for the PowerLogic ION meters

Resolution
We are currently not certified for calibration equipment per ISO 17025. Part of that standard is that all of our calibration houses are required to have it as well (i.e. 3rd party) and unfortunately not all of them currently offer it therefore Schneider Electric Labs that calibrate the PowerLogic ION meters are unable to attain it.

The ION meters are shipped from the factory with a certificate of compliance and calibration. In the event that you have lost it or did not receive one, a copy can be obtained by providing the meter's serial number and sending the request to technical support.
Was this helpful?
What can we do to improve the information ?