Technical FAQs

Ask a Question

Power Monitoring Expert 7.2.2 Floating License Manager activation error

Issue
While attempting to use the Floating License Manager to activate a new PME 7.2.2 standalone system installation, the following error is observed:

"The license activation component detected an error! Failed to activate the license. It is not allowed to activate the license in a virtual machine"

 
Product Line
Power Monitoring Expert 7

Environment
Power Monitoring Expert 7.2.2, Virtual Machine Hypervisor

Cause
The VM Hypervisor, operating system and SQL server versions are checked by the FLEXnet License administrator software. There cannot be unsupported virtual machine hypervisors installed on the server machine.

Resolution
Verify that there are no other virtual machine hypervisors installed on the server. The FLEXnet License Administrator software, which is used to manage StruxureWare Power Monitoring Expert licenses, supports virtual machine licensing for the following hypervisors:
  • VMware ESX 4.1/ESXi 4.1 and 5.0
  • Microsoft Hyper-V
  • Citrix XenServer 6.0
  • VMware Workstation 8.
Was this helpful?
What can we do to improve the information ?