Technical FAQs

Ask a Question

What is the mechanical life expectancy for the HMISCU relay output?

The mechanical life for the relay output on the HMISCU are rated for 20 million operation minimum at 25° C (77° F) for maximum current and voltage ratings

Was this helpful?
What can we do to improve the information ?