Technical FAQs

Ask a Question

What is the part number of the Panel PC 15-inch and 19-inch maintenance kit?

Issue:
What is the part number of the Panel PC 15-inch and 19-inch maintenance kit?

Product Line:
Magelis Panel PC

Environment:


Cause:


Resolution:
The part number for the maintenance kit is HMIYPNKT11.  It includes:
1 - 3-way removable connector for 24 V c power supply
1 - 3-way removable connector for 100…240 V a power supply
2 - protective covers for USB port on front panel (only on Aluminium bezel versions)
10 - replacement filters for fan, including:
5 - for Magelis Panel PC with no PCI slot
5 - for Magelis Panel PC with 2 PCI slots
18 - screw fasteners (Aluminium bezel) or 14 fasteners (Stainless steel bezel)
Was this helpful?
What can we do to improve the information ?