Technical FAQs

Ask a Question

Does the M241 controllers have Marine Certifications?

Issue:
Does the M241 controllers have Marine Certifications?

Product Line:
M241, TM241

Environment:


Cause:


Resolution:
Yes, the M241 controllers are Marine certified.  It has the following Marine certifications: ABS, DNV, GL, LR
Was this helpful?
What can we do to improve the information ?