Technical FAQs

Ask a Question

Is the IOC44 supported with CM3000 series meters?

Issue
Is the IOC44 supported with CM3000 series meters?

Product Line
CM3000 series meter

Cause
Customer wants to know if the IOC44 option card can be used with CM3000 series meters. 

Environment 
CM3000 digital inputs/outputs 

Resolution 
Yes, the IOC44 is an optional I/O card which can be installed in the CM3000 series meter. 

NOTE: The CM3000 series meter has only one slot which can be used for either the ECC21 or IOC44. As a result, if the customer already installed an ECC21 on a CM3000 series meter, then the customer will not be able to use the IOC44. Similarly, if customer has IOC44 mounted on CM3000 series meter, then the customer will not be able to use the ECC21. 
 
Was this helpful?
What can we do to improve the information ?