Technical FAQs

Ask a Question

Can you disable the O.P. switch on the XBTGH2460?

Issue:
Can you disable the O.P. switch on the XBTGH2460?

Product Line:
Magelis XBTGH2460

Environment:


Cause:


Resolution:
Yes, you can disable the O.P. switch.  To disable the switch operation (O.P.) of XBTGH, you must access the properties of the target, and disable the "operation switch".
 
Was this helpful?
What can we do to improve the information ?