Technical FAQs

Ask a Question

What is the maximum configuration for M251?

The M251 can have up to 7 TM3 /TM2 expansion modules and with the TM3XREC1 remote module and additional 7 TM3 expansion modules can be added.
The maximum number of TM4 expansion modules is 4.
Was this helpful?
What can we do to improve the information ?