Technical FAQs

Ask a Question

In Vijeo Designer, I change the target from an iPC to a non-iPC Magelis Panel. How come the font changed from a Windows font to Vijeo-S Albany?

Issue:
In Vijeo Designer, I change the target from an iPC to a non-iPC Magelis Panel.  How come the font changed from a Windows font to Vijeo-S Albany?

Product Line:
Vijeo Designer, Magelis iPC, HMIGTO/GTU/STO/STU, XBTG/GH/GK/GT,

Environment:


Cause:


Resolution:
If you change the target type to anything other than an iPC, it will change the font to Vijeo-S Albany.  That is because the non-iPC target, by default, does not have those Windows font as it is not an iPC target.

A work around would be to enable "Bitmap Display" on all Text Objects before converting them to a different target.  That will enable to Windows fonts in the non-iPC terminals for the Text Objects and that should resolve the issue.
 
Was this helpful?
What can we do to improve the information ?