Technical FAQs

Ask a Question

How to setup an auto or manual battery health test on an ADVC II controller?

A user would like to know how to setup an automatic test or run a manual test for battery health on an ADVC II controller

Product Line
ADVC II controller

Battery Health Test

1. Connect to the ADVC controller using WSOS software.
2. Navigate to maintenance--> Battery health test.
3. The battery health test can be set to run automatically by clicking the radio button for Auto and the frequency/start time can be updated as required.
4. The battery test can be started manually from the Manual Test menu as shown below.

NOTE: The manual battery test is grayed out if WSOS software is not communicating to the ADVC controller.

Was this helpful?
What can we do to improve the information ?