Technical FAQs

Ask a Question

Unity Pro: How to import sections, functionnal modules, variables, including DDDT without duplicating unusable DDDT?

When importing elements of application as sections, functionnal modules, variables, a screen « Import Trouble Report »  is proposed for variables which have same name in the element (source) to import and the application in which it has to be imported (destination).
If customer wants to use the DDDT variables from the source, he has to do the following choice :
- keep the name of the DDDT
- replace the elements of the DDDT
otherwise new DDDT will be created but could not be re-used.
 
Was this helpful?
What can we do to improve the information ?