Technical FAQs

Ask a Question

What is the correct replacement part number for the obsolete GBX080 008 1001F type gearbox?

Issue: Obsolescence


Product Line: BMH, BSH motors - Gearboxes


Environment: N/A


Cause: Gear box and Adapter kit needed to be ordered separately


Resolution:

Schneider Electric has changed the part numbering system for the GBX gearbox's used with the BMH, BSH motors

The gearbox has been separated from the mounting plate and now you will need to order these items individually.

The original part number of GBX080 008 1001F been replaced by the following

Gearbox part number = GBX 080 008K

Adapter kit for mounting gearbox to BMH/BSH 100x motor = GBK 080 1003F

 

Was this helpful?
What can we do to improve the information ?