Technical FAQs

Ask a Question

Can Cold Load Pickup be enabled even if Auto Reclose is disabled on an ADVC II?

Issue
A user would like to know if the Cold Load Pickup protection is independent of the Auto Reclose function on an ADVC II controller

Product Line
ADVC II recloser

Environment
Protection settings

Cause
Some protection features are dependent on Auto Reclose and cannot be enabled if Auto Reclose is disabled.

Resolution
Cold Load Pickup (CLP) is independent of Auto Reclose function and can be enabled even if Auto Reclose is disabled.

This can also be verified in the control tab of the recloser settings.



 
Was this helpful?
What can we do to improve the information ?