Technical FAQs

Ask a Question

How to find the IP address of a ADVC II controller and change it

A user would like to know the current IP address of the ADVC II controller and if needed change it.

Product Line
ADVC II Controller

10BaseT Ethernet communication IP address

Once connected to an ADVC controller, a user can navigate to Switchgear Communications--> Ports--> Port Configuration.

The current IP address and subnet mask is displayed on the left side of the pane and the new settings can be programmed on the right side of the pane and applied using the "Apply" button. 

Was this helpful?
What can we do to improve the information ?