Technical FAQs

Ask a Question

Is there a way to move a block of 16 IO point to a memory word in Unity Pro?

Yes.  
You can use the MOVE_AREBOOL_INT FB.
Depending on the Controller type, you can use the topological address:
MOVE_AREBOOL_INT (%I0.1.0:16,%MW1);

or the State RAM address:
MOVE_AREBOOL_INT (%I113:16,%MW1);

Make sure dymamic array addressing is enable in Unity Project setting --->Variables
 
Was this helpful?
What can we do to improve the information ?