Technical FAQs

Ask a Question

ION Enterprise 6.0 Web Reporter - Report Subscription - No Recipients Selected

Issue:
When a user attempts to add an email address in the distribution list, "No recipients selected" is observed even after an email address is saved.

Product Line:
ION Enterprise 6.0.x

Environment:
ION Enterprise 6.0.x Web Reporter - Report Subscriptions

Cause:
ION Enterprise 6.0.x Web Reporter does not support Internet Explorer versions 10 and 11.

Resolution:
ION Enterprise 6.0 Web Reporter is compatible with Internet Explorer versions 7, 8, and 9.

Uninstall Internet Explorer versions 10 and 11 or run Internet Explorer 10 or 11 in compatibility mode when viewing the Web Reporter page.

 
Was this helpful?
What can we do to improve the information ?